HVAC Glossary Of Terms

HVAC Glossary Of Terms

Glossary of terms

We’ve compiled this glossary to help you understand the different air conditioning/cooling/HVAC industry terms and acronyms used across our website and literature. Click on the alphabetical links below to jump to the appropriate section.

To download the glossary as a PDF document please click here.

If you find this glossary useful please link to our page from your website and feel free to Tweet and share on LinkedIn!

If there are any terms that you think we may have missed then please email them through to [email protected]

A B C D E F G H I K L M N O P R S T U V W Z

A.

Absolute pressure
Gauge pressure + atmospheric pressure. (Sometimes referred to with “a” on end – e.g. Bara, Psia.)

Accumulator
A storage tank that receives liquid refrigerant from the evaporator and prevents it from flowing back into the compressor.

AC fans
Fans of various types driven by an AC (alternating current) motor providing air movement in heating, cooling and ventilation systems.

ACIS™
Airedale Controls Integrated Systems (ACIS™) a building energy management system (BEMS) that operates and optimises a wide range of building services across multiple platforms and protocols. Also see BEMS.

ACRIB
Air Conditioning and Refrigeration Industry Board www.acrib.org.uk

Adiabatic cooling
Adiabatic cooling is the process of reducing heat through a change in air pressure caused by volume expansion.

Air conditioner
An appliance, system, or mechanism designed to control temperature, humidity and air quality in a defined space.

Air-cooled system
A type of air conditioning system that uses air as the transfer medium to reject heat from the refrigerant in the condenser. Typically, the air-cooled condenser is located and rejects waste heat to the outdoors.

Air diffuser  
Air distribution outlet or grill designed to direct and develop balanced airstreams.

Air handling unit (AHU)
A central unit consisting of fan(s), heating and cooling elements, filter racks or chamber, dampers, humidifier, and other central equipment required to provide suitable ventilation and extract. Also see our Air Handling Unit brochure.

Ambient
Normal atmospheric conditions of temperature & pressure

Application
Location or site where an air conditioning/cooling system or unit is to be installed (applied).

ASHRAE
American Society of Heating, Refrigerating, and Air-Conditioning Engineers www.ashrae.org

Azeotrope/azeotropic mixture
Product resulting from the combination of two or three compounds that have identical vapour and liquid compositions. An azeotrope cannot be separated into its parts by distillation. Azeotropes will fractionate slightly and experience temperature glide outside of the identified azeotropic points.

Azeotropic point
The temperature where a liquid mixture boils and produces a vapour with exactly the same composition as the liquid.

Back to top

B.

BEMS
Building Energy Management System is a computer-based control system installed in buildings that controls and monitors the building’s mechanical and electrical equipment such as ventilation, lighting, power systems, fire systems, and security systems. Designed to enhance system performance, drive down operational costs and aid decision making. Also see ACIS™.

Blend
A refrigerant mixture of two or more refrigerants blended in a specific ratio which can be separated by distillation. Regular blends may have up to 10°C or more temperature glide.

BREEAM
(Building Research Establishment Environmental Assessment Methodology) is the world’s longest established and most widely used method of assessing, rating, and certifying the sustainability of buildings www.breeam.org

British Thermal Unit (BTU)
The imperial measurement for the quantity of heat required to be given to or taken from 1lb. of water in raising or lowering its temperature by 1°F. This term is not commonly used other than on some equipment imported from the Far East or the USA.

Bubble point
The pressure at which a refrigerant liquid starts to vaporise.

Back to top

C.

Capillary tube
A metering device consisting of a small diameter tube designed to restrict flow. This is best used in constant ambient conditions.

Carbon Usage Effectiveness (CUE)
Carbon usage effectiveness (CUE) indicates the ratio of total CO2 emissions from the data centre to total IT equipment energy consumption. It is found by dividing energy consumption (converted to CO2 emissions) by IT energy consumption.

Cascade system
A system with two or more refrigerant circuits working in series to provide the designated level of cooling.

Cassette unit
Cassette air conditioning units are designed for commercial and residential applications. Ideal for large open plan areas or irregular shaped rooms they fit conveniently and discreetly into any area with a false or suspended ceiling.

Centrifugal compressor
A compressor with a rotating wheel which pushes the refrigerant outwards towards the rim of the wheel and from there to the condenser. It compresses gas using centrifugal force.

CFC
Chlorofluorocarbon (e.g. R12), high ozone depleting and global warming gases. Banned from 2000.

CFCs
Chlorofluorocarbons (CFCs) have been widely used as refrigerants. The manufacture and use of such compounds has been phased out and has been replaced with zero Ozone depleting products such as hydrofluorocarbons (HFCs).

CFM
The abbreviation for cubic feet per minute, the imperial measurement for the rate of air flow in an air conditioning system. This term is not commonly used.

Change of state
A change from one phase to another – solid, liquid or gas.

Chilled water system
A type of air conditioning system using water (or glycol solutions) as a secondary cooling medium. The primary cooling medium (refrigerant) is contained in a chiller, which is located remotely.  The chiller cools the water, which is then piped to the air conditioner to cool the space.

Chiller
chiller is a machine that removes heat from a secondary cooling medium (water, glycol solution, etc.) via a vapour-compression or absorption refrigeration cycle. The secondary cooling medium can then be circulated through a heat exchanger to cool air or equipment as required.

CIBSE
Chartered Institution of Building Services Engineers www.cibse.org

CITB
Construction Industry Training Board www.citb.co.uk

Clean room
A clean room is an environment, typically used in manufacturing or scientific research, with a low level of environmental pollutants such as dust, airborne microbes, aerosol particles, and chemical vapours.

Close control/Climate control
See Precision Air Conditioning (PAC) and Precision Air Conditioning.

Coil
Component providing heat transfer to air when mounted inside an air handling unit or ductwork. The term is normally associated with a fin and tube heat exchanger using refrigerant or water as the heat transfer medium.

Cold aisle
Cold aisle is a layout design for server racks and other computing equipment in a data centre. Cold aisle data center design involves lining up server racks in alternating rows with cold air intakes facing one way and hot air exhausts facing the other. The rows composed of rack fronts are called cold aisles. See Data Centre Aisle Containment for more information.

Comfort air conditioning
Comfort air conditioning systems are designed for the comfort of people, livestock, etc. and not for the protection of computer-based electrical systems or other process operations requiring close control of the environment.

Commercial air conditioning
Air conditioning for large buildings such as hotels, hospitals and other commercial buildings, providing suitable ventilation and space conditioning.

Commissioning
A service required after installation that ensures equipment is set up to function correctly, as per the specification, and to maximise system efficiently in order to provide optimal performance. Also see Commissioning.

Compressor
A key component of the refrigeration system, raising the pressure (and hence temperature) of the refrigerant and circulating it through a closed loop system.

Condensate
Moisture removed from the air when it is cooled below its dew point; normally associated with moisture removal during the dehumidification process in air conditioning.

Condenser
A vessel or an air cooled coil that removes the superheat of compression, condensing the refrigerant gas into a high pressure liquid.

Condensing unit
Part of a refrigeration/air conditioning system comprising a compressor, motor and condenser heat exchanger; supplied as a single unit to be matched with a suitable evaporator. Also see Condensers & Condensing Units.

Conduction
The transfer of heat by the movement of electrons or by the vibration of molecules through contact of two or more bodies of differing temperatures.

Constant air volume (CAV)
Constant Air Volume (CAV) is a type of heating, ventilating, and air-conditioning (HVAC) system. In a simple CAV system, the supply air flow rate is constant, but the supply air temperature is varied to meet the thermal loads of a space.

Controls
A control system that applies regulation to a heating and/or air conditioning system. A sensing device is used to compare the actual state (e.g. temperature) with a target state. Also see Controls.

Convection
The transfer of heat by changes of density in a fluid or gas as two fluid streams pass across each other.

Cooling tower
A water conservation device used to supply water for cooling condensers.

COP
Coefficient of performance (COP) is the ratio of the refrigerant effect (total capacity) versus the work by the compressor over a unit of time; the higher the number the more efficient the system.

CRAC
Computer Room Air Conditioning unit (see Precision Air Conditioning (PAC)).

CRAH
Computer Room Air Handling unit.

CWR
Chilled water return to a chiller.

CWS
Chilled water supply to a cooling unit.

Back to top

D.

Damper
A modulating device for controlling airflow rates through ductwork or air handling equipment.

Data Centre
data centre is a facility used to house computer systems and associated components, such as telecommunications and storage systems.

Decant/receiver
Clean empty cylinders for temporary storage of refrigerant during maintenance.

Dehumidification
The process of removing moisture from the air within a conditioned space to maintain the required humidity level.

Density
The weight of a unit volume of a substance.

Dew Point
The pressure/temperature where refrigerant gas starts changing from vapour to liquid phase. Also use to define te point where the air is saturated.

Direct Expansion Systems (DX)
This is a system using a refrigerant that passes through an expansion device prior to entering the evaporator. The system is used to extract heat in the evaporator and reject the waste heat through the condenser. This type of system is generally used in chillers, refrigerant based air conditioning systems and refrigeration equipment.

Downflow
Refers to a type of air conditioning system that discharges air downward, directly beneath a raised floor, commonly found in computer rooms and modern office spaces.

Drop-in
A gas that can be retrofitted into a refrigeration system designed for another, without major system changes. For example, R422D is a drop-in replacement for R22 in many applications. However, hydrocarbon refrigerants are NOT drop-in alternatives for most fluorocarbon refrigerants due to substantial system changes needed to manage their differing characteristics (e.g. flammability).

Duct
Ducts are used in heating, ventilation, and air conditioning (HVAC) to deliver and remove air including supply air, return air, and exhaust air.

Back to top

E.

EC fan
Electronically Commutated (EC) fans use brushless DC motors which include in-built electronics to convert the AC supply to DC without the need for a separate DC supply. EC fans provide a more efficient (up to 30%) means of airflow through Precision Air Conditioning (PAC) units with the additional benefit of variable speed control via an output signal from the unit controller. Also see EC Fan upgrades.

Economiser
An economiser is a mechanical device used to reduce energy consumption. Economisers recycle energy produced within a system or optimise environmental temperature differences to achieve efficiency improvements.

EER
Energy Efficiency Ratio (EER) is a measure of system efficiency at a given set of rating conditions. It is a ratio calculated by dividing the cooling capacity in kW by the power input in kW.

Electronic Expansion Valve (EEV)
This performs the same function as the TEV but provides closer control as the DC stepper motor opens and closes the valve in response to an output from the controller; maintaining very close control of the evaporator superheat. Also see Electronic Expansion Valves.

Energy Technology List (ETL) / ECA Scheme
The Enhanced Capital Allowance (ECA) Scheme is a key part of the Government’s programme to manage climate change. It provides businesses with enhanced tax relief for investments in equipment that meets published energy-saving criteria. See https://etl.decc.gov.uk/etl/site.html

Enthalpy
The thermodynamic property of a substance defined as its total internal energy plus the total heat & heat content Pv/J. Sometimes called total heat and heat content.

Entropy
The rate at which heat is absorbed into an object.

Energy Reuse Effectiveness (ERE)
Is the ratio of energy emitted from the data centre and reused elsewhere to total energy consumed. It is found by diving the amount of energy reused by the amount of energy consumed by the data centre overall.

Energy Reuse Factor (ERF)
Is the ratio of the data centre energy that is reused elsewhere in the facility and the total energy brought into the datacenter control volume (including IT, cooling, power, lighting etc.)

ESEER
As with EER, the Seasonal Energy Efficiency Ratio is a measure of equipment energy efficiency, but defined to suit the Europe market. Rather than using a single condition (EER) the SEER assumes four seasonal conditions for variable load performance of chillers, etc. and provides a suitable rating number for the equipment.

Evaporator coil
An evaporator coil is usually located indoors as part of a split unit or within an air handler or duct system. Inside the coil, refrigerant evaporates as it absorbs heat from the air that passes over it.

Evaporating temperature
The temperature at which a given refrigerant vaporises within an evaporator.

Expansion valve
A device that regulates the amount of refrigerant flowing from the liquid line into the evaporator. Can be a thermostatically operated valve, a capillary tube or a fixed orifice device.

Back to top

F.

Fan coil unit
A fan coil unit (FCU) is normally a chilled water device consisting of a heating and/or cooling coil, fan, valve/s and local controller. It forms part of a larger HVAC system found in residential, commercial, and industrial buildings.

F-Gas
Fluorinated gases (‘F-gases’) are a family of man-made gases used in a range of air conditioning and refrigeration applications. There are three types: hydrofluorocarbons (HFCs), perfluorocarbons (PFCs) and sulphur hexafluoride (SF6). These were produced in response to the need to eliminate ozone depleting gases.

F-Gas regulation
EU regulation introduced into European Law in 2007. Impacts the use of fluorine based refrigerants. Regulation leads to record keeping, leak detection and competence levels for engineers. See F Gas Compliance.

Filter-Drier
A device within a refrigeration system normally containing a desiccant designed to remove H2O.

Fluorocarbon
A chemical containing fluorine and carbon. Most refrigerants are classified as fluorocarbons – CFCs, HCFCs, HFCs and HFOs are all identified as this.

Footprint
The area or space that an air conditioning unit takes up when applied.

Free Cooling
This may apply to a system using fresh air for cooling the space or a water cooled or glycol cooled system with an additional coil that provides chilled water cooling when the outdoor ambient is cold; thereby reducing or eliminating compressor operation. These systems may provide free cooling for up to 80% of their operating life, particularly when operating in Northerly climates. See our Free Cooling page for more information.

Back to top

G.

Gauge pressure
The reading taken from a gauge normally zeroed at atmospheric pressure (one bar absolute or 14.7 psi) so that pressures can be also be read as a negative when below atmospheric pressure. (Often referred to with “g” on end – e.g. Barg, Psig).

Glide
The different boiling temperatures of the various components of a refrigerant blend, leading to a change in the relative components of the blend across a temperature range.

Glycol-Cooled System
A type of air conditioning system using a water/glycol solution as a condensing medium. Typically, the glycol-cooled condenser is located inside the air conditioner with the rest of the refrigeration components.  Water/glycol is piped to the unit from a drycooler or other suitable source. The glycol keeps the solution from freezing during winter operation.

GWP
Global Warming Potential, measure of global warming relative to CO2 = 1. CFCs often had GWP between 5,000 and 10,000. HCFCs and HFCs often have GWP between 1,000 and 4,000. Natural refrigerants and new HFO such as R1234yf normally have a GWP <20.

Back to top

H.

HCFC
Hydrochlorofluorocarbon (e.g. R22), lower ozone depleting, global warming gases.

Heat capacity
The amount of heat needed to raise the temperature of a given mass by 1 degree Kelvin.

Heat exchanger
A heat exchanger is a piece of equipment built for efficient heat transfer between two physically separated fluids.

Heat pump
A heat pump is a mechanical device that absorbs low grade heat from a lower temperature location and upgrades and transfers the resultant higher temperature medium, created by mechanical work, to heat a space to a sufficient comfort level. Heat pumps may be air to air, air to water, water to water or ground to water.

Heat transfer
Heat transfer describes the exchange of thermal energy between two interacting media passing through a heat exchanger, such as refrigerants, air and water.

Hemi-anechoic chamber
A room designed to completely absorb reflections of either sound or electromagnetic waves. Hemi-anechoic chambers have a solid floor that acts as a work surface for supporting heavy items such as large air conditioning units for testing sound levels. Also see Test chamber 4 – Hemi-anechoic chamber.

HFC
Hydrofluorocarbon (e.g. R134a), zero ODP, high global warming refrigerant gas.

HFO
Hydrofluoroolefin (e.g. R1234ze), zero ODP, low global warming, 4th generation refrigerant gas.

High Performance Computing (HPC)
High Performance Computing refers to the practice of aggregating computing power in a way that delivers much higher performance than one could get out of a typical desktop computer or workstation in order to solve large problems in science, engineering, or business.

Hot aisle
A hot aisle is a layout design for server racks and other computing equipment in a data centre. Hot aisle data centre design involves lining up server racks in alternating rows with cold air intakes facing one way and hot air exhausts facing the other. The rows the heated exhausts pour into are called hot aisles. See Data Centre Aisle Containment for more information.

Humidification
The process of adding moisture to the air within a space.

HVAC
HVAC (heating, ventilation, and air conditioning) is the technology of indoor and vehicular environmental comfort. Its goal is to provide thermal comfort and acceptable indoor air quality.

Hydrocarbon refrigerant (HC)
A family of chemicals containing only carbon & hydrogen that are suitable for use as a refrigerant. Common examples include propane (R290), isobutane (R600a), and the CARE range. Zero ODP, very low GWP.

Back to top

I.

Internet Service Provider (ISP)
An Internet service provider (ISP) is an organisation that provides services for accessing, using, or participating in the Internet.

Inverter compressor
This type of compressor uses an inverter drive to control the compressor motor speed to modulate capacity as demand varies.

Back to top

K.

Kilowatt (kW)
Measure of energy flow used to express the cooling capacity, heating capacity and power consumption of an air conditioning system.

Kyoto Protocol
International agreement to regulate global warming signed in Kyoto Japan. This sets out goals for reducing greenhouse gas emissions thought to be responsible for global warming. Likely to be the framework for further HFC usage restrictions.

Back to top

L.

Latent Cooling Capacity
The amount of energy added or removed from the air in order to increase or reduce the moisture content of the air during the air conditioning process.  It is measured in kg/kg of dry air.

Low pressure stage
The part of a single stage refrigerant system from the outlet of the expansion device to the compressor suction inlet. On a multi-stage system it is the part where the lowest temperature is achieved.

Back to top

M.

Make Up Air Unit (MUA)
Intake supply fan to replace air exhausted from a building. MUA may be heated or cooled so that the air coming in does not have a major impact on the building air conditioning systems, but is not designed to cool or heat the building.

Microchannel coil
The Microchannel coil design is based on technology from the automotive industry. It is constructed of parallel flow aluminium tubes that are mechanically brazed to enhanced aluminium fins, resulting in better heat transfer and a smaller, lighter, corrosion resistant coil.

Mineral oil
A lubricant commonly used with HCFC and HFC refrigerants, with a low affinity for moisture.

Back to top

N.

N+1
N+1 redundancy is a form of resilience that ensures system availability in the event of component failure. Components (N) have at least one independent backup component (+1).

Natural refrigerant
Non fluorochemical refrigerants, such as ammonia (R717), carbon dioxide (R744) and hydrocarbons such as propane (R290) or isobutene (R600a). These products exist naturally in the environment. Alternative to fluorochemical refrigerants, often used due to their low direct GWP and ODP potential. (However it should be noted that commercial production of natural refrigerants is normally via man-made synthesis).

Near azeotrope
This chemical product is formed by combining two or more compounds. Its vapour and liquid compositions are nearly identical. Near azeotropes have a temperature glide of less than 2ºC (ASHRAE 34 definitions).

Non-condensable gas
A gas in a refrigeration system that does not condense at the temperature and partial pressure that exists in the condenser, therefore leading to a higher head pressure. This is often the case if air has leaked into a system, and lowers system efficiency and leads to longer term reliability issues.

Back to top

O.

ODP
Ozone Depletion Potential, measure of damage to the ozone layer relative to R11=1. CFCs tend to have ODP between 0.1 and 1. HCFCs between 0.01 and 0.1. HFCs, HFOs and Natural Refrigerants = 0.

Oil separator
A device designed to separate oil from the refrigerant.

Back to top

P.

Packaged unit
A self-contained air handling unit made specifically for outdoor installation; it includes all heating and cooling devices pre-assembled prior to installation.

Precision Air Conditioning (PAC)
Precision Air Conditioning systems are primarily designed for process cooling such as data centre equipment or manufacturing rather than for the comfort of people. These systems offer excellent reliability and typically have a high ratio of sensible-to-total cooling capacity (COP).

Pressure and strength tests
Tests designed to prove the integrity of a system prior to evacuation and the addition of refrigerant.

Psychrometric Chart
The psychrometric chart represents factors relating to the condition of air and its change of state, based on 1kg of air.

PUE
Power usage effectiveness (PUE) is a metric calculated by measuring a data centre‘s total energy consumption divided by the energy consumption of its IT equipment. PUE values can range from 1.0 to infinity. Ideally, a PUE value approaching 1.0 indicates 100% efficiency, where all energy is used by IT equipment only.

Back to top

R.

R1234ze (HFO Refrigerant)
One of the ‘fourth generation’ refrigerants, R1234ze is a hydrofluoroolefin (HFO) based refrigerant rated by the International Panel for Climate Change (IPCC) with a GWP lower than one, better than CO2. It is seen as a replacement for R134a. Also see Low GWP refrigerant TurboChill™ R1234ze cools John Lewis.

R134a (HFC Refrigerant)
R134a (Tetrafluoroethane) is a haloalkane refrigerant with zero ozone depletion potential designed to replace R12. Its major usage is automotive air conditioning, refrigerators and chillers.

R22 (HCFC Refrigerant)
R22 is a refrigerant gas found in the majority of air conditioning equipment over 10 years old. R22 is a hydrochloroflourocarbon which have ozone depleting potential (ODP) if leaked into the atmosphere. The use of R22 for maintenance or repair will be banned from 1st January 2015.

R407C (HFC Refrigerant)
R407C is a zeotropic hydro-fluoro-carbon refrigerant and is a blend of difluoromethane (R32) providing the heat capacity, pentafluoroethane (R125) decreasing flammability and tetrafluoroethane (R134a) to reduce pressure. Difluoromethane serves to, pentafluoroethane andtetrafluoroethane. R407C was developed as a replacement for the ozone depleting R22.

R410A (HFC Refrigerant)
R410A is one of the third generation hydro-fluoro-carbon refrigerants designed to replace earlier ozone depleting substances.  It is a zeotropic, but near-azeotropic mixture of difluoromethane (CH2F2, called R32) and pentafluoroethane (CHF2CF3, called R125), which is used as a refrigerant in air conditioning applications.

Rack
A computer rack (commonly called a rack) is a metal frame used to hold various hardware devices such as servers, hard disk drives, modems and other electronic equipment.

Reclaim
The re-processing and upgrading of refrigerant by filtering, drying, distillation and sometimes chemical treatment of the recovered refrigerant. The re-processed substance will require laboratory analysis to verify that it meets a specific quality standard, normally that of new refrigerant. This normally involves processing “off-site” at a re-processing or a refrigerant manufacturing facility.

Recovery
Taking used gas out of a fridge system and filling it into packages. Avoids release into the environment – an action that is environmentally irresponsible and illegal in many countries. This process is usually performed by a refrigeration contractor. This occurs during maintenance or when removing a refrigerant permanently due to equipment decommissioning or retrofitting to a new gas.

Recycle
To improve the quality of recovered refrigerant before re-use. This is to clean refrigerant by oil separation, distillation and single or multiple passes through filter-driers to remove moisture, acidity and particulate matter. Recycling may be done on or off site.

Refrigerant
The fluid used for the heat transfer within a refrigeration system. The refrigerant absorbs heat at low temperature and pressure and transfers heat at high temperature and pressure. The refrigerant can be many materials, commonly fluorocarbon compounds, but also natural refrigerants such as ammonia, CO2, hydrocarbons as well as other compounds such as water and air.

Refrigerant charge
The amount of refrigerant in kg in a closed system.

Refrigeration Cycle (Vapour compression cycle)
The vapour compression refrigeration cycle is accomplished by continuously circulating a constant volume of refrigerant gas in a closed system. By varying pressure and temperature within different parts of the system the refrigerant absorbs waste heat from the conditioned space in the evaporator and rejects it through the condenser.

Relative Humidity (%rh)
Relative humidity is the ratio of the partial pressure of water vapour in an air-water mixture to the saturated vapour pressure of water at a prescribed temperature. In prevailing Northern European conditions relative humidity and percentage saturation (ration of moisture content) can be considered the same as the divergence is <1%.  In high temperature areas they should be treated differently as the divergence may be as high as 10%.

Remote Electronic Expansion Valve (REEV)
An EEV that can be installed with a remote control panel in purpose designed evaporators. Also see Electronic Expansion Valves.

Retrofit
To remodel the refrigerant system to improve the performance, i.e. fit new refrigerant gas, add energy saving components, etc.

RCI (HI) and RCI (LO)
The Rack Cooling Index (RCI) is a metric that measures the percentage of racks in the data centre where the air inlet temperature is at the recommended or allowable level under the guidelines put forth by ASHRAE. RCI (hi) is the metric for racks at the upper limit and RCI (lo) for racks at the lower limit. This metric reveals how uniformly and efficiently a data centre is being cooled.

R-number
Official number assigned to a refrigerant upon accreditation by ASHRAE.

Back to top

S.

Screw compressor
A Compressor utilising the action of two synchronised screws to pressurise the refrigerant vapour.  Typical capacities are 50 – 1000kW and they have a modulating performance band of between 10 and 100% making them particularly suitable for use in chillers.

Scroll compressor
A type of compressor fitted with two compliant scrolls, one fixed and one oscillating to compress refrigerant as it passes between them. Used extensively in air conditioning systems the scroll compressor may be fixed or variable capacity using digital unloading or inverter control.

Sensible Cooling Capacity
The amount of heat energy removed from the air without changing the actual moisture content of the air.

Sensible Heat Ration (SHR)
The ration of sensible heat to total heat.

Server
A server is a system that responds to requests across a computer network to provide, or help to provide, a network service.

Split System
A split air conditioning system consists of two main parts: the outdoor (condensing) unit and the indoor unit. Although any size of unit could be defined as a split system it normally refers to smaller equipment, specifically air to air heat pumps.

Sub cooling
The removal of heat from a liquid to a point lower than the saturation temperature at that pressure. This normally occurs in the condenser heat exchanger.

Super heating
Heating a vapour so that its temperature is higher than the saturation temperature at that pressure, e.g. steam at >100ºC is superheated.  This normally occurs in the evaporator.

Back to top

T.

Thermostatic expansion valve (TEV)
A precision control device, designed to control the evaporator superheat by regulating the rate at which liquid refrigerant flows into the evaporator.

Thyristor
A thyristor is a semiconductor device which can be used to switch electric currents and is often used to control the output of electric heaters.

Turning Vane
Turning vanes are devices inside mechanical ductwork used to smoothly direct air inside the duct where there is a change in direction, thus reducing resistance and turbulence.

Back to top

U.

Upflow unit
A type of air conditioning system that discharges air into the conditioned space via a top-mounted discharge plenum or through an overhead duct system.

UPS
An uninterruptible power supply (UPS) is an electrical apparatus that provides emergency power to a load when the input power source, typically mains power, fails.

Back to top

V.

Vacuum test
A test to check the gas tightness of a refrigeration system before charging it with refrigerant, by drawing a vacuum upon it.

Vapour
The gaseous form. In refrigeration terminology, often referred to gases at near equilibrium with liquid phase that does not follow gas laws – in gaseous state below the critical temperature.

Vapour barrier/seal
A vapour seal is an essential part of preventing moisture infiltration into or migration out of a critical space, such as a data processing centre or other room that contains sensitive electronic instrumentation.  Essentially, a vapour seal is a barrier that prevents air, moisture, and contaminants from migrating through tiny cracks or pores in the walls, floor, and ceiling into the critical space.  It is also used extensively on pipe insulation to prevent moisture ingress that may cause deterioration of the insulation or freezing in cold conditions.

Back to top

W.

Water-Cooled System
A type of refrigerant based air conditioning system that uses water as a condensing medium. Typically, the water-cooled condenser is located inside the air conditioner with the rest of the refrigeration components. Water is piped to the unit from a cooling tower or other suitable source.

Water Usage Effectiveness (WUE)
Is a site-based metric developed by The Green Grid that is an assessment of the water used on-site for a data centre’s operation. This includes water used for humidification and water evaporated on-site for energy production or for cooling the data centre and its support systems.

Watt
The watt is a derived unit of power in the International System of Units (SI), named after the Scottish engineer James Watt (1736–1819). The unit is defined as joule per second and can be used to express the rate of energy conversion or transfer with respect to time.

Wet Bulb Temperature
The wet-bulb temperature is the temperature a parcel of air would have if it were cooled to saturation (100% relative humidity) by the evaporation of water into it, with the latent heat being supplied by the parcel.

Back to top

Z.

Zeotrope
Refrigerant blends consisting of a combination of two or more different chemical compounds, often used individually as refrigerant for other applications. Unlike azeotropes, zeotrophic blends separate more easily into their original parts via distillation.

Contact Us to Learn More.