Back to top

Compressors

With more than 500 different compressors and compressor parts in stock, we have the UK’s largest stock holding of compressors available for immediate dispatch, making Airedale first choice for compressors in the HVAC industry.  

Our large stock holding means that there is no need to wait for overseas delivery, as we can provide you with the right compressor in the quickest time. We stock all the leading brands including Danfoss, Copeland, Emerson, Siam and can deliver the compressor you require directly to site within 24 hours. 

Our compressors can be used in single or tandem configurations and can also be modulated for increased efficiency. Whether it’s screw, scroll, centrifugal or the latest Turbocor compressors, we will find a compressor to best suit your requirements and will offer you the best advice and technical support.  

For further information on our compressors, see below or alternatively, please contact our spares team: spares@airedale.com



Types of compressors

Screw compressors

Screw compressor

Screw compressors offer excellent individual full and part load efficiency and provide good value for money. 

With low noise and vibration levels and few moving parts, screw compressors are extremely reliable. 






Scroll compressors

Scroll compressors

Scroll compressors are very quiet and compact compressors with few moving parts and low vibration levels. 

Their simple, oil-free design means that they require little maintenance and they are highly efficient at managing both part and full loads. 

They offer greater cooling capacity than other types of compressor, whilst also using less energy. 

For chiller operation, scroll compressors also provide better part load efficiency (IPLV) than chillers with a single large screw compressor and capacity controls.




 

Centrifugal compressors

Centrifugal compressor

These intelligent, self-optimising, oil-free compressors are ideal for use where there are high cooling capacities and low compression ratios. 

They enable variable speed control and minimise input power with near silent operation. 

Magnetic bearings within the centrifugal compressor levitate the compressor shaft and with no mechanical contact or friction between mating surfaces, the need for lubrication is eliminated.

These compressors offer excellent reliability and with virtually no vibration and fewer moving parts within the compressor, there is no operational wear and tear. 

Costly bearing replacement is therefore avoided and equipment life extended. 

In the event of a power failure, the compressor acts as a generator and powers itself down in a controlled manner. 



TG310 compressors

TG310 compressor

Revolutionary oil-free centrifugal TG310 compressors operate using the next generation low, global warming potential refrigerant R1234ze. 

R1234ze significantly reduces environmental impact and has a low global warming potential (GWP) of under one*. This means that the time taken for the refrigerant to break down and for it to be absorbed into the atmosphere is minimised. Therefore, the lifespan of the refrigerant R1234ze is just 16 days.  

See our John Lewis R1234ze case study

 

*As rated by the International Panel for Climate Change.



Order or make an enquiry below

  • Providing your email address means you will receive occasional news about Airedale innovations, products and services before anyone else, we will never share or sell your details to third parties and you can easily unsubscribe at any time.


  •