Airedale Launches AireWall ONE™
Airedale’s AireWall ONETM has been designed with input from industry experts, to deliver a flexible, efficient and global range of data center fan arrays for an industry striving for scalability and sustainability.
Airedale by ModineTM, the critical cooling specialists, has today announced the launch of AireWall ONETM, a fan wall developed in collaboration with the data center industry. AireWall ONE has built-in flexibility, with a parametric design allowing it to be configurable to physical space, and is designed to operate in sustainable facilities that prioritize energy efficiency. AireWall ONE will be manufactured in Spain, the UK and the U.S. for shipment globally.
AireWall ONE is a customer-led product, developed from the ground-up with considerable input from data center end-users, consultants and contractors alike. The new range capitalizes on the sustainability potential offered in data centers utilizing higher air and water temperatures, delivering energy efficiency benefits across the whole cooling system. A parametric configuration philosophy is at the heart of its design – with over 33,000 size permutations, clients can configure AireWall ONE to suit a multitude of construction and cooling requirements, within the following parameters:
- 200-650kW
- 2-12 EC centrifugal fans
- 6, 8 or 10 coil row options
- Configurable footprint to suit the space
Installation and maintenance teams were also heavily involved in the design process of AireWall ONE. Often overlooked in the R&D process, several contractor-friendly features have been designed into the range that simplify on-site manoeuvring, positioning, commissioning and in-service maintenance.
Paul Golding, Global CRAH and CRAC Product Manager for Airedale said, “Following an intense period of consultation with a range of industry specialists, we are delighted to launch AireWall ONE. This is an evolution of our previous AireWall range, improved to include the features that our clients have told us they now need as the industry continues to grow at an unprecedented rate.”
Paul continued,
“AireWall ONE bridges the gap between an effective fan wall and an intelligent, efficient computer room air handler. It has been designed to deliver a flexible, efficient and global solution to an industry striving for scalability and sustainability.
Paul concluded,
“Because it is a parametric design, clients can work with us to configure the units to their site and cooling design. Airedale is part of Modine, a global leader in thermal management and cooling solutions. Airedale leverages this capability and expertise to configure the chilled water coils to the size of the unit and the required cooling output for each project. Our engineering teams and global production sites are ready; we’re extremely excited to make this range available to all our clients worldwide.”
As with all Airedale cooling equipment, AireWall ONE is delivered with the latest helix™ intelligent controls platform and can be integrated into a complete intelligent cooling system using Airedale’s Cooling System Optimizer™ and ACIS™ facility management system.
For more information about AireWall ONE, please visit www.airedale.com
Ends
About Airedale
At Airedale, we believe that air conditioning has a critical role to play in an increasingly connected world. We also passionately believe that air conditioning equipment must play a responsible role in an era where sustainability is key to the preservation of our planet. Airedale is a global specialist in providing complete cooling solutions to industries where HVAC is mission critical, like data centres, healthcare, telecoms, education and pharmaceuticals. Our leading edge products, including chillers, close control and air handling units, are backed up with intelligent software solutions and complete applications and service support. With a strong R&D ethos rooted in sustainability and quality, Airedale’s 600+ employees are committed to providing experiences, products, service and solutions that support our clients in meeting their performance, efficiency and sustainability goals. Headquartered in Leeds, U.K. and with facilities in Consett (U.K.), Guadalajara (Spain), Dubai (UAE), Rockbridge (U.S.) and Grenada (U.S.), Airedale is part of Modine (NYSE: MOD), a diversified global leader in thermal management technology and solutions.
About Modine
At Modine, we are Engineering a Cleaner, Healthier World™. Building on more than 100 years of excellence in thermal management, we provide trusted systems and solutions that improve air quality and conserve natural resources. More than 11,000 employees are at work in every corner of the globe, delivering the solutions our customers need, where they need them. Our Climate Solutions and Performance Technologies segments support our purpose by improving air quality, reducing energy and water consumption, lowering harmful emissions and enabling cleaner running vehicles and environmentally-friendly refrigerants. Modine is a global company headquartered in Racine, Wisconsin (U.S.), with operations in North America, South America, Europe and Asia. For more information about Modine, visit www.modine.com.
Media Contacts:
UK: Nicola Ware | E: nicola.d.ware@airedale.com | Tel: +44 113 2391000
US: pr@modine.com