Airedale develops bespoke solution to solve DataCentre challenge

Airedale develops bespoke solution to solve DataCentre challenge

Airedale Air Conditioning, Leeds, UK, August 3, 2018

The Challenge

One of the biggest downtime threats for data centre operators is leaks, and  preventing them is one of the most fundamental areas of protection of data centres and critical facilities.

Standard technologies for leak detection include tape leak detection or pipe-in-pipe solutions. But what happens when the extent of the water distribution scheme and inaccessibility make these inapplicable?

This was the situation with one of the  largest data centres in the UK, who  have a water distribution system to feed 20MW of adiabatic cooling units.

They needed a solution to both solve this issue and which also adhered to the prestigious Tier IV certification requirements.

The Solution

Airedale developed the T4TWDS (The Tier 4 Treated Water Distribution  System). A bespoke solution to solve this issue.

The T4TWDS is both a mechanical and control solution, which monitors and controls water treatment, water storage and water distribution for adiabatic cooling units in a datacentre.

The solution designed was also capable – with a complex algorithm of volumetric flow monitoring – to detect leaks, faults and to isolate elements of the system to  ensure that service to the datacentres was never disrupted.

Key features included:

• A water flow meter that both monitored  flow and detected leaks at the same time. – automatically taking  action to verify and isolate the potential issue

• An additional infrastructure layer to the water distribution system, making water available via redundant monitored supplies to all of the cooling units at all times

• Reliability of the adiabatic system reduced the requirement of a mechanical cooling circuit to achieve cooling

• The system was self-adjusting to specific conditions and faults, to guarantee that service was never disrupted.

The T4TWDS was engineered for resilience and reliability levels that are common in mission critical applications but unlikely to be connected to other water distribution systems. This was achieved with distributing intelligence to every controller and outstation, making them capable of functioning independently or sharing functionalities with the other controllers.

The Results

Energy efficiency savings – Mechanical cooling was only required for “topping up” the available cooling. For the majority of time the adiabatic system in the units was used achieving a PUE of 1.1.

The solution also received two BREEM points in recognition of its low global warming impact.

Ease of maintenance – Planned maintenance was more easily carried out because of automated features of the solution including  seasonal drain down, auto-leak shut down, and automatic leak checking.

Overall reduction in costs – The solution could be integrated into the site’s existing BMS system and because of the resilience and intelligence of the system there were less call-outs.

Client Testimonial – Well known datacentre facility management company

“Airedale’s commitment to achieve the best possible results has been impressive. Lead by a strong management team, the engineers have worked to produce a project of the very highest standard in terms of functionality and craftsmanship.

There have been, as with most projects, obstacles and anomalies materialising, which in its self, is common practice. The professional approach to deal with these is the difference between good and exceptional contractors, which Airedale have proved themselves to be.”

In summary, Airedale have been proud to work on this project and are delighted to be able to solve this particular challenge. We pride ourselves on developing bespoke solutions to challenging industry problems.

Contact Us For More Information

The owner of this website has made a commitment to accessibility and inclusion, please report any problems that you encounter using the contact form on this website. This site uses the WP ADA Compliance Check plugin to enhance accessibility.