Testimonials

Testimonials

Airedale by Modine are trusted globally in some of the world’s most demanding HVAC applications, delivering thermal management to iconic projects and mission critical environments.

Customer Testimonials

From offices to shopping centres, military installations to nuclear power stations and telecoms cabins to hyperscale data centres, Airedale by Modine are trusted by clients based all over the world to deliver and support their critical HVAC systems.

We have worked with some of the world’s largest and most prestigious organisations. Our enviable customer list of end users, contractors and consultants speaks for itself and Airedale prides itself on a partnership approach, developing long term relationships and engaging throughout a project lifecycle from initial design through to installation, commissioning and installed base support.

Corscale 150x68
1763_fullimage_EDF-Energy-Logo
EDF Energy is already seeing a PUE of 1.2. I believe we are the first company in the world to install Airedale’s advanced technology, the TurboChill™ free cooling chiller. When the data centre is operating in free-cooling mode, the PUE has been measured at 1.2 and we expect that to reduce further as we install more equipment.
1766_fullimage_EMIS-Logo
The InRak™ makes the aisle containment far more efficient. The InRak™ units are very clever; they communicate with each other to maintain pressure and temperature consistent in the room. Their EC fans are linked to the ACIS™ and ramp up and down according to demand. ACIS™ gives us 24/7 control of the operation and peace of mind. When fully populated, Airedale’s cooling solution should guarantee an annualised PUE of 1.3 for the room.
1762_fullimage_Epson-Logo
Our target is to reduce building energy costs by 7% annually which we have achieved over the past two years. Airedale’s free cooling chillers are already contributing to 3% of this annual saving. We make the equipment work through a complete and positive partnership with Airedale, from design through to service and maintenance.
We have a positive, responsible partnership with Airedale in which we share knowledge. It is only through Airedale’s continued site involvement that we can fi ne tune the system to such an extent. We don’t mind spending capital expenditure to recoup such significant energy savings as these.
1760_fullimage_Harrogate-Borough-Council-Logo
Our priority at the Harrogate Hydro leisure facility is to provide the comfortable environment which our customers have come to expect. A major concern was to find a reliable, appropriate air conditioning system which would keep a cool, constant temperature within the building. Airedale’s chilled water chiller and cassette solution is delivering that.We have a positive, responsible partnership with Airedale in which we share knowledge. It is only through Airedale’s continued site involvement that we can fi ne tune the system to such an extent. We don’t mind spending capital expenditure to recoup such significant energy savings as these.
1761_fullimage_IBM-Logo
Airedale listens to our requirements as a customer and adapts its products to suit us. The beauty of Airedale’s solutions is that they are designed to grow with the application.
1765_fullimage_Iceland-Logo
Iceland Frozen Foods (IFF) has realised savings of £1.5m to date. The typical payback is between six and nine months per store, making Airedale Controls’ solution extremely attractive operationally and financially. Its flexibility has enabled IFF to carry out a progressive implementation strategy, integrating existing Airedale equipment, as well as new and old systems from other OEMs.
1769_fullimage_LDeX-Logo
Continued operation of our clients’ IT infrastructure and ensuring availability of their data is paramount. Airedale provides us with a fully integrated cooling solution designed for maximum efficiency and critical redundancy. Airedale’s latest chilled water and DX cooling technologies enables us to achieve our PUE target of less than 1.3.”\
1767_fullimage_The-National-Gallery-Logo
Airedale gives us support and reassurance throughout. A factor influencing selection of Airedale was its transparency and facility to witness test. We prefer working with a UK manufacturer who is carrying out product development work and can give us support and reassurance throughout.
1764_fullimage_University-Of-Leeds-Logo
Our HPC facility is growing and without the use of the OnRak™ rear door heat exchangers it would not be possible to go to such high densities. The OnRak™ has saved us space in an already densely packed environment. It has also given us the flexibility to fit rear door heat exchangers to legacy or new cabinets from any manufacturer.
1768_fullimage_ybs_retail_logo
Energy efficiency was the crucial factor. Airedale proved that its free cooling chiller can save energy and is the right system for us. Anything that improves payback is of interest to the Society. We have also had good service from other Airedale products.
Quality_Innovation_thumb

QUALITY & INNOVATION

Innovative product development is key to Airedale’s success, setting air conditioning industry standards when it comes to manufacturing expertise and addressing industry, economic and environmental challenges.

Test_Centre_thumb

TEST CENTERS

Airedale has invested in a multi-million pound 1,323m² purpose-built facility that sets the standard as one of the most advanced air conditioning product testing centres of its kind, and one of the biggest in Europe.

Environment_thumb

ENVIRONMENT

Airedale are known as a company that always tries to push the boundaries of technology, investing into research & development with a focus on energy efficiency and the environment.lit.

The owner of this website has made a commitment to accessibility and inclusion, please report any problems that you encounter using the contact form on this website. This site uses the WP ADA Compliance Check plugin to enhance accessibility.